Floating License Installation: 1. Redeem > 2. Server > 3. Client

Setting up a Floating License Client PC

After configuring the floating license server, use Keysight Manager 6 to access the floating licenses.

  1. Install Keysight License Manager 6 on the Client PC.

  2. Launch the client PC's Keysight Manager 6 from the Windows Start menu.

  3. Select Specify a remote floating license server from License Manager 6's startup menu.

  4. Select SIGNALSTUDIO in the drop-down product menu and click OK. (This step could be skipped automatically if there is no other related product pre-installed on the client PC.)

  5. Enter the license server's full name preceded by the "@" symbol. (e.g., @myserver.mycompany.com).

  6. Click Next. License Manager 6's License Setup Wizard will connect with the floating license server and discover its licenses.

  7. Click Done when you see a message that the licensing actions were successful.

  8. Click the View licenses and License usage tabs to check the available licenses on the newly connected server.